Page tree

Download the StruxureWare Portal below.

The StruxureWare Portal is available for

Compatible with DCO

Download Portal version

DCO 8.1.0

Windows: StruxureWarePortal-1.3.7.exe

Linux: linux-installer-1.3.7.zip

Add-on (without Liferay installation): StruxurewarePortal.1.3.7_ce.zip

DCO 8.0.4

Windows: StruxureWarePortal-1.3.6.exe

Linux: linux-installer-1.3.6.zip

Add-on (without Liferay installation): StruxurewarePortal-1.3.6_addons.zip

DCO 8.0.2 and 8.0.3

Windows: StruxureWarePortal-1.3.5.exe

Linux: linux-installer-1.3.5.zip

Add-on (without Liferay installation): StruxureWarePortal-1.3.5_addons.zip

DCO 8.0.1 and 8.0.2

Windows: StruxureWarePortal-1.3.4.exe

Linux: linux-installer-1.3.4.zip

Add-on (without Liferay installation): StruxureWarePortal-1.3.4_addons.zip

DCO 8.0.0

Windows: StruxureWarePortal-1.3.3.exe

Linux: linux-installer-1.3.3.zip

Add-on (without Liferay installation): StruxureWarePortal-1.3.3_addons.zip

DCO 7.5

Windows: StruxureWarePortal-1.3.2.exe

Linux: linux-installer-1.3.2.zip

Add-on (without Liferay installation): StruxureWarePortal-1.3.2_addons.zip

   

Release news and user assistance for the StruxureWare Portal is available here.

Skip to end of metadata
Go to start of metadata
  • No labels
RELATED COMMUNITY QUESTIONS
WAS THIS ARTICLE HELPFUL?